AXIS#.VL.ARZF1 TO AXIS#.VL.ARZF4

Description

AXIS#.VL.ARZF1 sets the natural frequency of the zero (numerator) of AR filter 1. This value is FZ in the approximate transfer function of the filter:

ARx(s) = [s²/(2πFZ)² +s/(QZ2πFZ) + 1]/ [s²/(2πFP)² +s/(QP2πFP) + 1]

The following block diagram describes the AR filter function; note that AR1 and AR2 are in the forward path, while AR3 and AR4 are applied to feedback:

AR1, AR2, AR3, and AR4 are used in velocity and position mode, but are disabled in torqueTorque is the tendency of a force to rotate an object about an axis. Just as a force is a push or a pull, a torque can be thought of as a twist mode.

Discrete time transfer function (applies to all AR filters)

The velocity loop compensation is actually implemented as a digital discrete time system function on the DSP. The continuous time transfer function is converted to the discrete time domain by a backward Euler mapping:

s ≈ (1-z-1)/t, where t = 62.5 µs

The poles are prewarped to FP and the zeros are prewarped to FZ.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

Hz

Range

5 to 5,000 Hz

Default Value

AXIS#.VL.ARZF1: 5000 Hz

VLARZF2 to VLARZF4: 500 Hz

Data Type

Float

Stored in Non Volatile Memory

Yes

Variants Supported

All variants are supported

Fieldbus Information

FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design Parameter Index Sub-Index Data Type Float Scale Units Access PDO Mappable
EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen AXIS1.VL.ARZF1 0x5011 0x18 UDINT 1000:1 - RW False
AXIS1.VL.ARZF2 0x5011 0x19 UDINT 1000:1 - RW False
AXIS1.VL.ARZF3 0x5011 0x1A UDINT 1000:1 - RW False
AXIS1.VL.ARZF4 0x5011 0x1B UDINT 1000:1 - RW False
AXIS2.VL.ARZF1 0x5111 0x18 UDINT 1000:1 - RW False

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen